{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are some appropriate steps to troubleshoot an inoperative transformer?
Issue:
How to troubleshoot a Dry type EE or EX transformer?

Product Line:
transformer

Environment:
EE and EX transformers

Cause:
trouble shooting incorrect voltages, wiring issues, odd or weird voltages to ground, or inoperative transformer

Resolution:
1. Check that line and load connections are properly made and that appropriate jumpers and/or tap settings are in accord with nameplate instructions.
2. Measure input voltage to insure that voltage is within 5% of nominal rated voltage or tap setting
3. If input circuit protection opens while energizing transformer, make sure fuse or circuit breaker is a minimum 1.25 x full load input current rating of the transformer.
4. If the transformer can be energized, measure output voltage with no load on transformer to insure that voltage is within tolerance.
5. If a neutral is derived on the load side of the transformer, insure that neutral ground bonding is accomplished in accord with National Electric Code or local code requirements. Failure to ground neutrals is often the cause of unusual voltage measurements to ground.


 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.