Search FAQs
Can the operating handle of a J250DS circuit breaker enclosure be padlocked in the ON position?
Issue:
Product design features
Product Line:
Circuit Breaker Enclosures
Resolution:
The provisions to padlock the operating handle in the ON position is not a standard feature of the enclosure. A factory special modification can be ordered that will provide the padlock ON capabilities; add suffix SPLO to the standard catalog number (J250DSSPLO). For field modification, a 3/8 inch maximum hole can be drilled in the lockoff slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability.
Product design features
Product Line:
Circuit Breaker Enclosures
Resolution:
The provisions to padlock the operating handle in the ON position is not a standard feature of the enclosure. A factory special modification can be ordered that will provide the padlock ON capabilities; add suffix SPLO to the standard catalog number (J250DSSPLO). For field modification, a 3/8 inch maximum hole can be drilled in the lockoff slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability.
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: