Search FAQs
On the LRD LR3D series overloads, what is the LAD7C1 used for ?
Issue:
Use of LAD7C1
Product Line:
Contactors and Starters-IEC
Environment:
Tesys D contactors
Resolution:
It is a pre wiring kit to allow direct connection of the NC contact of relay LRD01-D21 or LR3D01-D21 to the contactor.
Use of LAD7C1
Product Line:
Contactors and Starters-IEC
Environment:
Tesys D contactors
Resolution:
It is a pre wiring kit to allow direct connection of the NC contact of relay LRD01-D21 or LR3D01-D21 to the contactor.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: