{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many auxiliary contact blocks can be mounted on the LC1F contactor?
Issue:
Number of contact blocks that can be stacked on the right side of an LC1F contactor.

Product Line:
Tesys F Contactors

Environment:
IEC Contactors and Starters

Resolution:
A maximum of two contact blocks ( 1, 2 or 4 contact ) can be mounted on the right side. There can also be a single circuit block on the left hand side.

Schneider Electric Canada