{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the U-line self protected starter be used as a combo starter?
Issue:
Wants to use the U-line self protected starter as a combo starter.

Product Line:
Tesys U Enclosed Combination Starter

Environment:
IEC Contactors and Starters

Resolution:
Yes. It conforms to UL508E as a self-protected device when a LU9SP0 incoming line phase barrier is used.

Schneider Electric Canada