{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many 9999SX11 or SX12 internal auxiliaries can fit into a 8502/8536SAO** thru SDO** contactor or starter ?
Issue:
How many 9999SX11 / SX12 internal auxiliaries can be used on Type S Contactors/Starters from size 00-2?

Product Line:
Type S Accessories and Components

Environment:
NEMA and Definite Purpose Contactors and Starters

Resolution:
One additional 9999SX11 or SX12 can be put into a lower right cavity in the base of these Size 00 thru 2 contactors . There is one 9999SX11 in the upper left cavity as standard for holding circuit purposes . If 2 wire control is used, this upper left interlock is free to be used for other electrical signaling.

Schneider Electric Canada