{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Catalog number for the field-installable 110-130V Under voltage (UV) trip for the Powerpact H, J or L frame breakers.
Issue:
Can the 120v UVR Accessory for H, J and L Powerpact breaker be field installed ?

Product Line:
Powerpact H, J, L Breaker

Environment:
Application

Cause:
Product Features

Resolution:
The field installable Undervoltage trip accessory is part number is S29406.

Schneider Electric Canada