{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we offer a IEC reversing contactor that is rated for elevator duty?
Issue:
Is there any elevator duty contactor?

Product Line:
TeSys D contactors

Environment:
IEC TeSys D contactors

Resolution:
We do not offer a contactor with specific ``elevator rating`` however IEC devices are certainly suitable for this type of application. Specific duty ratings such as this are usually obtained by the OEM. We do offer certain sizes of IEC contactors with CSA listing for elevator use.

Schneider Electric Canada