{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the CH364DS, series F5? (may be shown as F05)
Issue:
Previous Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The replacement parts for the CH364DS, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056703550 (1 required; includes Phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
Line Base mounting screws - 4020514202 (6 required per line base)
Load Base Assembly - 4056678250 (1 required per phase; includes Phenolic base, lugs, and fuse clips)
Load Base mounting screws - 4020514202 (2 required per load base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (includes 6 lugs; requires mounting screws)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires mechanism coupling assembly 4056699850 and interlock connector assembly 4056718850)
Switch Mechanism mounting screws - 2194918121 (2 required)
Handle Assembly - 4056736850
Lockplate - 4056738901
Lockplate mounting screws - 2194918121 (2 required)

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: