{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the 9001 Type BF control station come with a back box?
Issue:
Back box on control station

Product Line:
Push Buttons and Operator Interface

Environment:
9001B Control Stations

Resolution:
No, supply the back box separately. Uses standard 2.0 inch or 2.13 inch deep wall boxes. Single gang box for types BF1 and BF2 and two gang box for type BF3.

Schneider Electric Canada