{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum amperage breaker available that can be installed into the largest size I-Line panel?
Issue:
Largest amp size breaker

Product Line:
Panelboards

Environment:
I-Line

Cause:
Maximum rating

Resolution:
The highest bus rating for I-line panels is 1200A. Because of this, the largest breaker available to plug on to the I-Line bus is also 1200A. However, a breaker this large can only be used on the HCR-U type panelboards.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: