undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
My SR3B101BD will not communicate with an SR3MBU01BD because of Error Code 60. What does "Error Code 60" mean under the module diagnostics menu?
Issue:
Identify the meaning of an "Error Code 60" in the module diagnostics menu for Smart relay SR2/SR3

Product Line:
Zelio Logic Smart Relays

Environment:
SR2/SR3 Zelio Smart Relays

Resolution:                                                                 
Under the module diagnostics menu "Error Code 60" means:
At the beginning of RUN on the smart relay application, the program is incompatible with the bus extension physically connected to the power supply.
 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top