{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the replacement melting alloy overload relays for a 8810SEO2 2-speed starter?
Issue:
What is the replacement overload for the class 8810 Size 3, 2 speed starters? (Melting alloy overload)
Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Two-speed Starter

Resolution:
9065SDO12 for the three pole starter and a 9065SDO14 (Obsolete) for the 5 pole starter.

Schneider Electric Canada