{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is fuse part number A155F1DSR0100E for a quantity of one or three?
Issue:
Is A155F1DSR0100E used for 3 fuses?

Product Line:
Switchboards and Switchgears

Environment:
Medium Voltage Metal-Enclosed Switchgear

Resolution:
This part number is for one fuse. The fuses in the Digest are for a set of three. This fuse in a set of three would be part number 15GS100.

Schneider Electric Canada