{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Square D manufacture 'Dummy' breakers to fill empty tenant breaker spaces in a Meter Pak device with 125amp Meter sockets?
Issue:
Product Design features

Product Line:
Meter Pak metering

Environment:
accessories

Cause:
Application

Resolution:
Yes Square D does offer QO type 'Dummy' breakers, it would require two(2) of part number QO1DB per tenant breaker position. BUT a dummy breaker should not be required if the tenant breaker will not be used, the customer can just close and lock the front tenant breaker cover.

Schneider Electric Canada