{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there plastic covers for the Mini Aluminum power distribution blocks?
Issue:
What is the part number for the plastic cover for a 9080LBA361101?

Product Line:
Power distribution blocks

Environment:
Power Distribution blocks, North America

Cause:
What is the part number for the plastic cover for a 9080LBA361101?

Resolution:
Schneider offers the following miniature power distribution blocks:

Miniature Aluminum Power Distribution Blocks

Lug Wire Range [1]

Aluminum [2]

Main

Branch

One Pole

Two Pole

Three Pole

Type

Type

Type

(1) #14–2

(1) #14–2

LBA161101

N/A

LBA361101

(1) #14–2

(4) #18–10

LBA161104

LBA261104

LBA361104


with the following covers available:

Clear Plastic Covers (0.045 in. thick)

For LBA Type[4]

Type

Dim. A

Dim. B

LBA161...

LB11

0.824

2.31

LBA261...

LB12

1.459

2.31

LBA361

LB13

2.094

2.31

Schneider Electric Canada