Issue:
Repair parts
Product Line:
HD Safety Switch
Resolution:
The repair parts for the HU364AWK, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704050 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line/Load Base mounting screws - 4020546401 (requires 6 per line base)
Arc Suppressor Assembly - 4056677550 (requires one per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (requires 2)
Handle Assembly - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Repair parts
Product Line:
HD Safety Switch
Resolution:
The repair parts for the HU364AWK, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704050 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line/Load Base mounting screws - 4020546401 (requires 6 per line base)
Arc Suppressor Assembly - 4056677550 (requires one per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (requires 2)
Handle Assembly - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Released for:Schneider Electric Canada