{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a QO/QOB GFCI circuit breaker available with shunt trip, auxiliary contacts, or alarm switch?
Issue:
Can a QO or QOB GFCI circuit breaker be ordered with shunt trip, auxiliary contacts, or an alarm switch, or can they be field installed?

Product Line:
Circuit Breakers

Resolution:
QO/QOB-GFI breakers are available with aux contacts or an alarm switch, but there is no shunt trip option available.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: