Search FAQs
Are alternate mechanical lugs available for the EZM1800CB, Series M01 main breaker device?
Issue:
Product Design Features
Product Line:
Metering Equipment
Resolution:
The EZM1800CB Series M01 uses the MHP26800 main breaker and the standard lugs for this breaker accept (3) 3/0 AWG to 500 kcmil AL/CU wires per phase and (4) 3/0 AWG to 500 kcmil AL/CU wires for the main neutral.
The alternate PHASE lugs for the MH frame circuit breaker used in this device are:
(2) AL800MA7 terminals, where each terminal will accommodate two 500 - 750 kcmil AL/CU wires, or
(2) AL1000MA terminals, where each terminal will accommodate four 1/0 AWG - 350 kcmil AL/CU wires.
Alternate NEUTRAL lugs for this device include:
(1) MMLK250 kit that includes (3) 2-Barrel lugs, two of these 2-Barrel lugs can be use on this neutral in place of the standard neutral lugs. Wire range will accommodate (2) 1/0 AWG - 600 kcmil AL/CU, or (4) 1/0 AWG - 250 kcmil AL/CU.
NOTE: One extra 2-Barrel lug remains from this kit and will not be used.
For (2) 750Kcmil Max. Al/Cu wires per phase and neutral a MMSK2 lug landing kit and (2) TA8002N (manufactured by ILSCO, Purchased separately). When installing on the neutral, use the PHASE pads from this kit, which will have a small offset. DO NOT use the pad with the large offset that is marked with the letter 'N'
Product Design Features
Product Line:
Metering Equipment
Resolution:
The EZM1800CB Series M01 uses the MHP26800 main breaker and the standard lugs for this breaker accept (3) 3/0 AWG to 500 kcmil AL/CU wires per phase and (4) 3/0 AWG to 500 kcmil AL/CU wires for the main neutral.
The alternate PHASE lugs for the MH frame circuit breaker used in this device are:
(2) AL800MA7 terminals, where each terminal will accommodate two 500 - 750 kcmil AL/CU wires, or
(2) AL1000MA terminals, where each terminal will accommodate four 1/0 AWG - 350 kcmil AL/CU wires.
Alternate NEUTRAL lugs for this device include:
(1) MMLK250 kit that includes (3) 2-Barrel lugs, two of these 2-Barrel lugs can be use on this neutral in place of the standard neutral lugs. Wire range will accommodate (2) 1/0 AWG - 600 kcmil AL/CU, or (4) 1/0 AWG - 250 kcmil AL/CU.
NOTE: One extra 2-Barrel lug remains from this kit and will not be used.
For (2) 750Kcmil Max. Al/Cu wires per phase and neutral a MMSK2 lug landing kit and (2) TA8002N (manufactured by ILSCO, Purchased separately). When installing on the neutral, use the PHASE pads from this kit, which will have a small offset. DO NOT use the pad with the large offset that is marked with the letter 'N'
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: