Search FAQs
Are EZM bussed corner sections available?
Issue:
Are EZM bussed corner sections available?
Product Line:
Bussed Corner Section
Resolution:
Yes, but they are only available in a NEMA 1, indoor enclosure.
The bussed, inside corner sections offered are EZM1CORNER (1 phase, 3 wire) and EZM3CORNER (3 phase, 4 wire).
The bussed outside corner sections offered are EZM1ELBOW (1 phase, 3 wire) and EZM3ELBOW (3 phase, 4 wire).
All units are supplied with 1200 A, copper, horizontal cross bus, but can interconnect with other EZM devices supplied with 800 A copper or aluminum horizontal cross bus.
Are EZM bussed corner sections available?
Product Line:
Bussed Corner Section
Resolution:
Yes, but they are only available in a NEMA 1, indoor enclosure.
The bussed, inside corner sections offered are EZM1CORNER (1 phase, 3 wire) and EZM3CORNER (3 phase, 4 wire).
The bussed outside corner sections offered are EZM1ELBOW (1 phase, 3 wire) and EZM3ELBOW (3 phase, 4 wire).
All units are supplied with 1200 A, copper, horizontal cross bus, but can interconnect with other EZM devices supplied with 800 A copper or aluminum horizontal cross bus.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: