{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can GVAE1, GVAE11 or GVAE20 be used with GV3 starters?
Issue:
Are the front mount auxiliary contacts GVAE1, GVEA11 and GVAE20 be used for GV3M devices?

Product Line:

Tesys GV Manual Starter and Protectors

Environment:
TeSys GV, GVA, GV2, GV3P

Resolution:
These auxiliary contacts can only be used with the rotary handled GV3P devices. They cannot be applied with the pushbutton GV3M devices.

Schneider Electric Canada