{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is there a plastic guard available for ZB5 or ZB4 - 40mm EMO Operators?
Issue:
What is the catalog number for a plastic yellow guard for ZB5 or ZB4 - 40mm EMO Mushroom Operators?

Product Line:
Push Buttons and Operator Interface

Environment:​
XB4 and XB5 22 mm operators

Resolution: 
ZB4BZ1905 is the standard round plastic yellow guard; ZB4BZ2005 is the narrow flange guard.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top