{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a QO generator panel be used as a sub panel by using only one circuit breaker as the main and ignoring the generator connection?
This unit could be used as a sub panel, but may not pass inspection because it is labeled as an actual generator panel. The label states it is to be fed by a dual power supply, and may have to be connected as such. This depends on the discretion of the local inspector.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: