Search FAQs
What is the catalog number for a sensor plug for a Powerpact P, R, or Masterpact NW, NT breaker?
Issue:
Need Sensor plug catalog number
Product Line:
Circuit Breakers
Resolution:
Note: See 2nd table for Masterpact Y frame (6p) replacement sensor plugs.
Need Sensor plug catalog number
Product Line:
Circuit Breakers
Resolution:
Note: See 2nd table for Masterpact Y frame (6p) replacement sensor plugs.
Rating (Amps) | Part # |
---|---|
100(*) | S47051 |
250(*) | S47052 |
400 | S47053 |
600 | S48823 |
630 | S33091 |
800 | S33092 |
1000 | S33093 |
1200 | S48824 |
1250 | S33094 |
1600 | S33095 |
2000 | S33982 |
2500 | S33983 |
3000 | S48825 |
3200 | S33984 |
4000 | (IEC and ANSI) S47820 |
* Cannot be installed into a circuit breaker with original sensor plug higher
than 250 A. Likewise, a circuit breaker with original sensor plug of 100 A or
250 A cannot be replaced with a sensor plug higher than 250 A.
Installation Notes:
Masterpact NT and NW: Sensor plugs are field installable down to 50% of the FRAME rating.
Example: Masterpact with a 1600 A frame can receive sensor plugs from 800-1600 A.
Powerpact P and R: Sensor plugs are field installable down to 50% of the CURRENT rating.
Example: Powerpact P frame breaker with 800 A sensor installed at the factory can only receive sensors from 400-800 A.
For complete details on installing sensor plugs and their restrictions, please see instruction bulletin 48049-145-03.
than 250 A. Likewise, a circuit breaker with original sensor plug of 100 A or
250 A cannot be replaced with a sensor plug higher than 250 A.
Rating (Amps) | Part # |
---|---|
2000 | S47821 |
2500 | S47822 |
3000 | S48826 |
3200 | S47823 |
4000 | S47824 |
5000 | S47825 |
6000 | S48827 |
6300 | S47826 |
Installation Notes:
Masterpact NT and NW: Sensor plugs are field installable down to 50% of the FRAME rating.
Example: Masterpact with a 1600 A frame can receive sensor plugs from 800-1600 A.
Powerpact P and R: Sensor plugs are field installable down to 50% of the CURRENT rating.
Example: Powerpact P frame breaker with 800 A sensor installed at the factory can only receive sensors from 400-800 A.
For complete details on installing sensor plugs and their restrictions, please see instruction bulletin 48049-145-03.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: