{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are 600 A double throw safety switches provided with a service ground kit?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches(DTSS)

Resolution:
Yes, ALL the 600 A double throw switches include (3) #6 - 250kcmil wire size ground lugs as standard. For the replacement ground kit, order catalog number DS468GKD.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: