{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do the LC1D40 through LC1D95 contactors mount on DIN rail?

Issue:
Can LC1D40-95 be Din-rail mountable?

Product Line:
Contactors and Starters-IEC

Environment:
Tesys D contactors

Resolution:
Yes. They will mount on 35mm DIN or 75mm DIN. In some cases it will require two sections of 35mm.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: