Search FAQs
What is the complete through the door operating mechanism for the PowerPact M and P frame breakers?
Issue:
What is the complete thru the door operating mechanism for the PowerPact M and P frame breakers?
Product Line:
Operating Mechanisms
Environment:
Type L Circuit Breaker Mechanism
Resolution:
Mechanism with standard shaft and 8`` handle is part number 9421LW1 and with long shaft operating mechanism is part number 9421LW4.
What is the complete thru the door operating mechanism for the PowerPact M and P frame breakers?
Product Line:
Operating Mechanisms
Environment:
Type L Circuit Breaker Mechanism
Resolution:
Mechanism with standard shaft and 8`` handle is part number 9421LW1 and with long shaft operating mechanism is part number 9421LW4.
Released for:Schneider Electric Canada
Explore more
Product:
Range:
Explore more
Product:
Range: