Search FAQs
Are the 8501RS34 and 8501RSD34 Relays Rated for use in Hazardous Locations?
Issue:
Need to know if the 8501RS34 or 8501RSD34 relays can be used in hazardous environments.
Product Line:
Relays and Timers
Environment:
8501 General Purpose Relays
Resolution:
The 8501RS34 and 8501RSD34 relays are hermetically sealed and suitable for use in Class 1 Division 2 locations.
Need to know if the 8501RS34 or 8501RSD34 relays can be used in hazardous environments.
Product Line:
Relays and Timers
Environment:
8501 General Purpose Relays
Resolution:
The 8501RS34 and 8501RSD34 relays are hermetically sealed and suitable for use in Class 1 Division 2 locations.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: