{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the 9999BLX required when mounting a 9999SC2 into an 8536 Size 00, 0, or 1 Starter in a NEMA 1 enclosure?
Issue:
What is required when mounting a 9999SC2 into an 8536 Size 00, 0, or 1 Starter in a NEMA 1 enclosure?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Accessory

Cause:
Product Specification

Resolution:
The 9999BLX bracket is NOT required when mounting a 9999SC2 with the NEMA Starter.  The 9999SC2 includes a bracket which allows the switch to be mounted directly to the contactor.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: