{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there sub-feed lug kits available for RTI, Ready to Install, NQ panelboards?
Issue:
Does Square D provide sub-feed lug (SFL) kits available for RTI, Ready to Install, NQ panelboards?

Product Line:
Panelboards

Environment:
NQ panelboards

Cause:
Product features.

Resolution:
Yes, sub-feed lug kits are available for RTI NQ main lug only interiors. Refer to the NQ Digest pages available on line for selection and to determine if the box and trim sizes are impacted by adding sub-feed lugs.

Schneider Electric Canada