Search FAQs
Does the 2510 Type F starter come with the thermal unit mounting screws?
Issue:
2510 Type F starters heater screw
Product Line:
Manual Starters and Switches
Environment:
Manual Starters, Type F—Fractional Horsepower
Resolution:
No. Thermal unit mounting screws are included with the Type A thermal units.
2510 Type F starters heater screw
Product Line:
Manual Starters and Switches
Environment:
Manual Starters, Type F—Fractional Horsepower
Resolution:
No. Thermal unit mounting screws are included with the Type A thermal units.
Thermal unit mounting screws:
Use for TU A.22 thru A2.57, 2qty, 21916-14140
Use for TU A2.81 thru A25.2, 2qty, 21916-14121
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: