{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which trip units can be tested with the S33595 full function test kit (FFTK)?
Issue:
Trip units to be tested with FFTK

Product Line:
Molded Case and Air Circuit Breakers

Resolution:
The FFTK full function test kit can test the following Compact, PowerPacT, and MasterPact breakers and respective trip units:

Compact NS, NSJ breakers with these trip units:
  • STR22ME, STR22GE, STR22SE
  • STR23SE, STR23SP
  • STR43ME
  • STR53UP, STR53UE

PowerPacT M, P, R, and MasterPact NT, NW breakers with these trip units:
  • ET 1.0
  • ET 1.0I
  • ET 1.0M
  • 2.0, 3.0, 5.0
  • 2.0A, 3.0A, 5.0A, 7.0A
  • 5.0P, 5.0H, 7.0P, 7.0H
  • 6.0A, 6.0P, 6.0H

Schneider Electric Canada