{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I get the report generator software for the S33595 FFTK (full function test kit)?
Product Line:
Molded case and insulated case circuit breakers

Resolution:
To obtain that software, you may purchase the CD with it, part number FFTKRPT-V1-0 (FFTKRPTV10) or may download the attached file.

NOTE: A customer supplied serial (RS-232) cable is also required to connect from the FFTK to the computer.

NOTE: The software does not work on Windows 8 or Windows 10, and there are no plans to update it to work on those OS.

Schneider Electric Canada

Attachment(s)
FFTK Report Generator (1).zip [7.12 MB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: