{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the duplex receptacle ratings in the 9070SK transformer disconnects?
Issue:
Duplex receptacles for the 9070SK transformer disconnects

Product Line:
9070 Transformer disconnects

Environment:
Products sold in North America

Resolution:
The receptacles are two sizes depending on secondary current:
Up to 1500VA, with 120V secondary the units are supplied with 120V, 15A receptacles
Above 1500VA, they are supplied with 120V,  20A receptacles.
Circuit protection for the receptacles is sized accordingly

Schneider Electric Canada