{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a QED switchboard be ordered in a NEMA 4X enclosure? What options for the enclosure are there ?
Issue:
Can a QED switchboard be ordered in a NEMA 4X enclosure?

Product Line:
QED SWBD

Environment:
Application

Cause:
Product clarification

Resolution:
No. QED Switchboards are not available in NEMA 4X enclosures. They can be made in NEMA Type 1 or Type 3R enclosures only.

Schneider Electric Canada