{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is an automatic transfer switch (ATS) available for the Homeline load centers, similar to the QO used with Kohler generators?
Issue:
Product availability

Product Line:
Homeline Load Centers

Resolution:
No, there is no ATS feature for the Homeline load centers. That is ONLY available for the QO load centers at this time. The ATS, along with ALL the other components for the generator application, are ONLY available from a Kohler dealer/distributor.

Schneider Electric Canada

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: