{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is a lock off available for the EDB, EGB, and EJB breakers?

Article available in these languages: Spanish

Product Line:
Circuit Breakers

Resolution:
There is a removable padlock attachment that can be used on any series E-frame breaker:
HPAFD for lock ON and OFF

There are also fixed padlock attachments available for series 2 and higher E-frame breakers:
EDPA for lock ON and OFF
EDPAF for lock OFF only

These padlock attachments are also available factory installed (only available for fixed padlock attachments):
Suffix YQ = Lock OFF only
Suffix YP = Lock ON or OFFF

The EDPA must be attached to the breaker using slots in each end of the breaker escutcheon.
Standard EDB circuit breakers (series 2 and higher), have these slots (see picture below).

EDPA EDPA lock off

EDPAF EDPAF lock


For EDPA see instruction bulletin, 48840-256-01.
For EDPAF see instruction bulletin, 48840-255-01.
For HPAFD see instruction bulletin, 48840-080-01.

Schneider Electric Canada