Issue:
Would like to know if the U line is UL 508 Rated
Product Line:
Contact and Starters - IEC
Environment:
North American Products
Resolution:
UL 508 is a broad standard that covers industrial control equipment. The U line, being UL listed, complies with the relevant parts of the standard. In addition to the standard rating compliance , the U-line self protected version LUB12, LUB32 is UL508 Type E compliant when the incoming line phase barrier, LU9SP0, is installed.
Would like to know if the U line is UL 508 Rated
Product Line:
Contact and Starters - IEC
Environment:
North American Products
Resolution:
UL 508 is a broad standard that covers industrial control equipment. The U line, being UL listed, complies with the relevant parts of the standard. In addition to the standard rating compliance , the U-line self protected version LUB12, LUB32 is UL508 Type E compliant when the incoming line phase barrier, LU9SP0, is installed.