Issue:
Application
Product Line:
Canadian Generator Panel
Cause:
Application
Resolution:
NO, These load center Generator Panels can ONLY be used with unbonded generators since they do not switch the neurtal, which is a code requirement in Canada.
NOTE: The load centers will have a label on them that will state "Suitable for use ONLY with generators which have an UNBONDED NEUTRAL".
Application
Product Line:
Canadian Generator Panel
Cause:
Application
Resolution:
NO, These load center Generator Panels can ONLY be used with unbonded generators since they do not switch the neurtal, which is a code requirement in Canada.
NOTE: The load centers will have a label on them that will state "Suitable for use ONLY with generators which have an UNBONDED NEUTRAL".