{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the catalog number of a replacement joint pack for I-Line II busway?

Issue:
Replacement joint pack for I-Line II busway

Product Line:
Product sold in United States

Environment:
I-Line II busway

Cause:
Product Selection

Resolution:
The catalog number of a replacement joint pack begins with the prefix of the busway device`s catalog number and ends with a ``JP``. For example, the replacement joint pack for an AP2525G10ST would be an AP2525GJP. Another example would be a CFH2340GG44LES20B24 would need a replacement joint pack CFH2340GGJP.



Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: