{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the CH361DS, series F6? (may be shown as F06)
Issue:
Current design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The repair parts for the CH361DS, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056642050 (arc suppressor not included)
-Load Base Assembly - 4056002550K
-Line & Load Base mounting screw - 4020516001 (3 for line and 2 for load)
-Arc Suppressor Assembly - 4056669451
-Arc Suppressor mounting screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Keps Nut - 2342501701 (per lug)
-Mechanism Assembly - 4056610750
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056699450 (also recommend replacing lockplate gaskets)
-Lockplate - 4056693201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 (2 required)
-Ground Lug Mounting Screw - 4020513503
-Fuse Pullers - FPK03 (1 required)

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: