{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an HOM816U200FTRB, Series S02?
Issue:
Repair parts list for HOM816U200FTRB, series S2

Product Line:
Load Centers

Resolution:
Only the parts listed below are considered field replaceable:
Cover - 4056317550 (includes hinges attached to left side of cover)
Cover Mounting Screw - 2142217101 (2 required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (attached to right side wall of enclosure)
Interior Trim with Labels - 4056313301K
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM816U200FTRBI
Neutral Bonding Screw - 4028345850K
Main Lugs Kit/Main Breaker - This load center is a universal main device, which has no main lug or breaker installed. Field install QOL225 for main lug. Field install  QOM2100VH (100 amp), QOM2125VH (125 amp), QOM2150VH (150 amp), QOM2175VH (175 amp) or QOM2200VH (200 amp) for main breaker.
Note: Covers and Interior Trims do not have labels applied.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: