{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the catalog number for the closing plate that can cover the rectangular opening in an NQMB2Q main breaker adapter kit.

Issue:
Closing plate to fill in main breaker opening left in a NQMB2Q deadfront when the main breaker is removed or not used

Product Line:
NQ Panelboard

Environment:
Products sold in North America

Resolution:
If the NQ Main breaker interior, which contains the Q frame Main breaker, needs to be converted to a MLO interior, the NQMB2Q main breaker kit with deadfront, needs to be removed
and replaced with the NQ12RDE 12" rail extension kit with Blank deadfront.  The interior already has line lugs so no additional lug kit would be required to terminate incoming cable.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: