Search FAQs
Can more than one surge breaker be put in a panel? Looking at the QO2175SB.
Issue:
Can more than one surge breaker be installed in a single panel, for example, the QO2175SB?
Product Line:
TVSS Surge Suppression
Environment:
Application, installation
Cause:
Is it possible to install more than one surge protective device in one panel?
Resolution:
Yes, you can put more than one per panel, which will increase protection.
CTA-ID : 2044316
Can more than one surge breaker be installed in a single panel, for example, the QO2175SB?
Product Line:
TVSS Surge Suppression
Environment:
Application, installation
Cause:
Is it possible to install more than one surge protective device in one panel?
Resolution:
Yes, you can put more than one per panel, which will increase protection.
CTA-ID : 2044316
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: