{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Mechanical interlock for use with a NEMA size 4 and 5 8502 or 8536 Type S device?
Issue:
What is the part number to mechanically interlock one NEMA Size 4 and one NEMA size 5 Contactor/Starter?

Product Line:
NEMA Contactors/Starters

Environment:
Type S Contactors and Starters

Resolution:
31099-009-50

Schneider Electric Canada