{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a PowerPact H or J frame circuit breaker including either a GFM ground fault module or ELM earth leakage module be installed into any of the J250 enclosures?
Issue:
Can a PowerPact H or J frame circuit breaker including either a GFM ground fault module or ELM earth leakage module be installed into any of the J250 enclosures?

Product Line:
PowerPact H and J frame molded case circuit breakers with GFM ground fault modules or ELM earth leakage modules

Resolution:
We do not have any enclosure available for the PowerPact H or J frame breakers with either the GFM or ELM installed. Consider using in an I-Line panelboard application or use a Hoffman style box.
See the attached installation instructions for minimum enclosure dimensions.

Schneider Electric Canada

Attachment(s)
ELM 48041-089-01.pdf [6.14 MB]
HJ GFM 48041-088-01 Rev 3-10.pdf [2.48 MB]