Search FAQs
What tenant breakers do the EZM, 225amp Max. meter socket branch devices accept, both 3-Phase and 1-Phase?
Issue:
Current product design
Product Line:
EZM Metering
Environment:
Tenant breakers
Cause:
Product features
Resolution:
The EZM 225amp meter socket branch devices will ONLY accept as standard, Type QBP-TM, QDP-TM, QGP-TM or QJP-TM circuit breakers from 70A minimum to 225A maximum. The 1phase IN-1phase OUT and the 3phase IN-1phase OUT devices will use 2pole tenant breakers and the 3phase IN-3phase OUT will use 3pole tenant breakers.
NOTE: There is a adapter kit that does allow for the use of a 2pole, QO tenant breaker to be used in the single phase ONLY 225amp meter socket branch devices, catalog number EZM125QOA, BUT see the current digest for a description and the Short Circuit Current Rating of the ENTIRE EZM-Line when this kit is used.
CTA-ID : 2042723
Current product design
Product Line:
EZM Metering
Environment:
Tenant breakers
Cause:
Product features
Resolution:
The EZM 225amp meter socket branch devices will ONLY accept as standard, Type QBP-TM, QDP-TM, QGP-TM or QJP-TM circuit breakers from 70A minimum to 225A maximum. The 1phase IN-1phase OUT and the 3phase IN-1phase OUT devices will use 2pole tenant breakers and the 3phase IN-3phase OUT will use 3pole tenant breakers.
NOTE: There is a adapter kit that does allow for the use of a 2pole, QO tenant breaker to be used in the single phase ONLY 225amp meter socket branch devices, catalog number EZM125QOA, BUT see the current digest for a description and the Short Circuit Current Rating of the ENTIRE EZM-Line when this kit is used.
CTA-ID : 2042723
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: