{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a replacement Transformer or breaker panel only for an MPZ Mini Power Zone product?

Issue:
Transformer and breaker panel sections of an MPZ Mini Power Zone

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone Transformers by SquareD/Schneider Electric

Cause:
Replacement  parts needed for a Mini Power Zone product

Resolution:
A replacement Transformer for a Mini Power Zone product is available by special order based on the catalog number.
The outer Breaker Panel cover and some internal components are also available, depending on catalog number.
However, the outer sheet metal enclosure for the Breaker Panel is not available as a replacement part.

Schneider Electric Canada