{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are accessory lugs available for changing the various conductor sizes or increasing the number of conductors for Main Lug Only I-Line panels?
Issue:
Can the the number of conductors for Main Lug Only I-Line panels be increased?

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboards

Resolution:
No. The I-Line Main Lug Only interiors are UL listed to use only the lugs that they are shipped with. There are no expansion accessory lug kits available for them.

Schneider Electric Canada