{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use a NC68VS vented cover on a 250A NF Main Breaker panel that has a subfeed breaker and 30 circuits?
Issue:
250A NF Main Breaker panel with subfeed breaker and 30 circuits, can be mounted on NC68VS vented enclosure cover?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. Vented covers are used on 400A panels and above. You must use a NC68S.

Schneider Electric Canada